Part Number: LAUNCHXL2-570LC43
Tool/software: Code Composer Studio
Hi all, this is my main code for interfacing internet router through an ethernet cable. I saw a tutorial video of TI and done my coding. There was no errors but still i am not getting any data from router. I am attaching the screenshot of the console to get more detailed information. What can i do?
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
#include "HL_system.h"
#include "HL_gio.h"
#include "HL_sci.h"
/* USER CODE BEGIN (1) */
extern void EMAC_LwIP_Main (uint8_t * emacAddress);
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
/* USER CODE END */
uint8 emacAddress[6U] = {0x00U, 0x08U, 0xEEU, 0x03U, 0xA6U, 0x6CU};
uint32 emacPhyAddress = 1U;
void main(void)
{
/* USER CODE BEGIN (3) */
gioInit();
EMAC_LwIP_Main(emacAddress);
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
/* USER CODE END */