Part Number: TMS570LS3137
Hi,
I asked a related question about one month ago. The thread can be found at:
https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/938274
This thread was did not solve my problem. I still got the prefetch entry. I did the changes that mentioned in the above thread.
I looked at IFSR. İt is 0x409, addressing ECC error. The fault address is 0xC. I enabled and disabled ECC and tried running, got prefetch entry again.
The interesting thing is, when I debug and put breakpoint to Fapi function in disassembly window and step one by one, the code is working. Also, when I tried to write another bank, the code working. However, I cannot write/erase in same bank. Also, I checked in disassembly window, Fapi functions run from RAM. Is there any idea for solution.
Osman,
Thanks in advance.