Part Number: TMS570LS0914
Other Parts Discussed in Thread: TMS570LC4357
In the question that this one refers to, there is an answer that asks me to look at the MSE bit in the RAMCTRL register. I infer that when this is set, if a single bit error is corrected, the corrected version is written back to the memory. But I do not see that bit in RAMCTRL in my MTR. Does this only exist in some TMS570 processors? Does that mean that in my processor, if there is a corrected error, I should write it back myself to reduce the probability of a double-bit error?