Part Number: MSP432P401R
Other Parts Discussed in Thread: UNIFLASH
Hi,
I get this error message on two of my MSP432p401r launchpads after doing the following:
1. I've attempted an encrypted update, with writing the SWD/JTAG lock mailbox, although the device was not locked. After reboot the device never came online. At that point I might have pushed the board reset button.
2.1 I've SWD/JTAG locked the device, written the flash mailbox to do a secure update. I've used ResetCtl_initiateHardResetWithSource() to reboot
2.2 It rebooted to my original code, with the correct source.
2.3 It was running for a while, at which point, I've pushed the reset button on the board. From that point onward I don't see any code running. and I get this error.
In both cases I get this error message. Nothing I could find online matched my situation, I can not connect or do a factory reset in a way described here. If my code would be running I could factory reset it, by shorting a GPIO. I've tried Uniflash Version: 6.0.0.2710, gives the same message. Practically no matter which function I select (tried: unlock, factory reset, manual flash erase, blank check etc..).
I've also tried switching debugging to JTAG in CCS, with no success.
The code used has been used in the past successfully with some changes.
There is no mention of the error code here: software-dl.ti.com/.../emu_xds110.html
What state it is in now? How can I clear the error? I've bricked two boards, so I'm reluctant to try my last board.
Thanks,
Peter