Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C129EXL: ROM Bootloader via Ethernet

Part Number: EK-TM4C129EXL
Other Parts Discussed in Thread: EK-TM4C1294XL

SW-TM4C-BOOTLDR-UG-2.2.0.295 states:

  1. When the user application is running, it can still invoke the ROM boot loader to force an update of the firmware through a chosen interface.
  2. Before calling the ROM boot loader API, the application must configure and enable the chosen interface and disable all processor interrupts.

I have the enet_tcpecho_server examle (provided in TivaWare_C_Series-2.2.0.295) running which has been modified to call ROM_UpdateEMAC(SYSCLK) when a message is receieved. I have called MAP_SysTickIntDisable, MAP_EMACIntDisable, and IntMasterDisable prior to calling the bootloader, but unable to download a new application via LM Flash Programmer once the bootloader has been entered.

Can you advise as to what I'm missing please.

Thanks

HL