Part Number: RM57L843
Dear TI' support,
I need to connect 12M size of MRAM memory to RM57 processor.
MRAM is MR5A16A so it's 16b and I think of connecting four of them to EMIF interface.
since the address range of MR5A16A is [20:0] then my idea is to use AND gate with ADDR[21] and nCS signal to select particular chip.
so one AND gate, two MR5A16A chips could serve on single nCS.
eventually I'm going to use nCS2 and nCS3 to connect four MRAM chips, and have nCS3 left for connecting flash memory.
please kindly check if my idea has no issues other than impossibility to use 8bit pointer.
similar topic I found on TMS570, but designer had no intention to use so big memory space.
below you can find electrical connection schematic diagram of my idea.

thank you in advance,
Wojciech