Part Number: ARM-CGT
Other Parts Discussed in Thread: TMS570LS2124, TMS570LS1224
Hello All,
In previous follow up I was told to include the option --float_support=VFPv3D16 to have the compilation of Code on R4F, My complete options are
'Invoking: ARM Compiler'
"E:/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="E:/ti-cgt-arm_16.9.6.LTS/include" --include_path="E:/XXXX_R4" --define=PREPROC_SW_TEST_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=packed --abi=eabi --preproc_with_compile --preproc_dependency="YYY/XXXXX.pp" --obj_directory="YYY" "../YYY/XXXX_R4.c"
Now I am facing problem in basic floating point operation like multiply\divide
for eg
uint64_t u40PowerInLinSum;
float fRecipEnerLinSum,dRangeOffset, dVelocityOffset;
fRecipEnerLinSum = (float)((float)1.0 /(float)u40PowerInLinSum); //u40PowerInLinSum value is 1612388
dxxOffset = (float)si32xx * fRecipEnerLinSum; //si32xx -687948
dyyOffset = (float)si32yy * fRecipEnerLinSum; //si32yy 640046
Result of above operation is fRecipEnerLinSum is 0, dxxOffset and dyyOffset 0x20202020, I checked these result in watch and also in the memory as sometime the watch shows wrong result
All this result is resulting in junk results.
I saw during compilation I use --float_support=VFPv3D16 what is the meaning of this and will this enables the floating point operations or not?
Or I am doing something wrong
Br
Deepak Joshi