This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a question for Errata MEM#03 and MEM#04 which are revision 6 Errata.
For both Errata, below workaround is available.
- Limit the number of lifetime EEPROM writes to 7 writes per word.
Suppose EEPROM is programmed once in customer factory, then no Erase nor Write operations happen after that,
both Errata can be avoided, correct?
These Errata are applicable the cases the number of lifetime writes are more than 7?
Thanks and regards,
Koichiro Tashiro