Part Number: TM4C123FE6PM
I have read this thread: Non Volatile Memory Lifetime / Endurance
what will happen at the end? is the data retention just get lower and lower but it is still function?
I have an application where I use the flash basically as extra temp buffer since the RAM is limit. I need to write to it more that 100K per day. what will happen after a year? will it still retain the data for a few minutes while it has the power connected?