Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi everyone,
I'm trying to use arm compiler 9.3.1 for TMS570LC43 board but the compiling doesn't successful since the arm compiler 9.3.1 libraries are compiled in LE.
If anyone can help me out it would be so appreciated.
Below the error logs:
C:/ti/ccs1011/ccs/tools/compiler/gcc-arm-none-eabi-9-2020-q2-update-win32/bin/arm-none-eabi-gcc-9.3.1.exe" -mfpu=vfpv3-d16 -O2 -g -gdwarf-3 -gstrict-dwarf -Wall -specs="nosys.specs" -mbig-endian -mcpu=cortex-r5 -Wl,-Map,"TMS570LC4357_GCC_Example.map" -mcpu=cortex-r5 -mfpu=vfpv3-d16 -mfloat-abi=hard -mbig-endian -o"TMS570LC4357_GCC_Example.out" ...............ect.
makefile:164: recipe for target 'TMS570LC4357_GCC_Example.out' failed
c:/ti/ccs1011/ccs/tools/compiler/gcc-arm-none-eabi-9-2020-q2-update-win32/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: c:/ti/ccs1011/ccs/tools/compiler/gcc-arm-none-eabi-9-2020-q2-update-win32/bin/../lib/gcc/arm-none-eabi/9.3.1/thumb/v7+fp/hard/crti.o: compiled for a little endian system and target is big endian
...
etc.
BR
Andrea