Part Number: TM4C1294KCPDT
Why is it sensitive to capacitor and resistance of 25MHz X-TAL?
For example, if 10pF X 2 units are installed, the operation for 30 minutes is changed to 22pF, and it will be down 1 minute after the call is connected.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294KCPDT
Why is it sensitive to capacitor and resistance of 25MHz X-TAL?
For example, if 10pF X 2 units are installed, the operation for 30 minutes is changed to 22pF, and it will be down 1 minute after the call is connected.
Hi,
Please refer to the device datasheet in section "Main Oscillator Specifications" for detail. It explains how the C1 and C2 are calculated. There is also table listing part numbers of crystals that have been simulated and confirmed to operate within the specifications of the main oscillator input characteristics. The table includes the NX5032GA-25.000MHZLD-CD-1 crystal which is used in the reference design. Normally, customer should consult the vendor of the crystal supplier for the proper C1/C2 to use.