Hi experts,
Could you let us know information about CPUSEL0 register ?
DataSheet(revD) describes below Table 8-9. C28x Bus Master Peripheral Access
about "Secondary Masters" and "CPU1 and CPU2 subsystem"
Is CPUSEL0 related with them ?

TRM : CPUSEL0 , a user can select which CPU is connected with each ePWM
For an example,
CPU1 : ePWM 1, 2, 3, 16 are assigned( = a user software control), sync source ePWM16
CPU2 : ePWM 4, 5, 6 are assigned, sync source ePWM16
In this case, which CPU should connected ?
Best regards,
Hidehiko