Part Number: TMS320F28388D
Hello,
I am using F28388D controller, i have a question on the bus contention for this controller between CPU1 and CPU2 for Peripherals Fame 1:
I am referring TRM SPRUII0B : May 2019–Revised May 2020
From the Bus architecture i understand as below :
11.6 CPU and CLA Arbitration
• Peripheral frame 1: ePWM, eCAP, eQEP, SDFM, CMPSS, DAC
• Peripheral frame 2: PMBus and SPI
Conflict Example: The CLA is accessing DAC-A while the DMA is simultaneously accessing DAC-B.
Conflict Example: The CPU is accessing an SPI FIFO while the DMA is simultaneously accessing a
PMBus register.
Non-conflict Example: The CPU is accessing a shared ePWM while the DMA is accessing an SPI.
The above text explains arbitration is required if we use CPU, along with its DMA , CLA.
My question here is if i use ePWM in CPU1 and eCAP in CPU2 do we still need the arbitration logic. Do they have independant bus ?
thanks,
Nagesh