This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello support team,
I'm confused between RAM & FLASH based linker file.
if I use RAM based linker file (e.g. 28002x_generic_ram_lnk.cmd), all the code will be written to RAM area of the device, and that means, the code will be deleted after a power reset. Is that correct?
Does it also mean that we only use RAM based linker file for testing because of higher speed, and for end of line product we have to use FLASH based linker file (with ramfunc attribute if needed)?
Regards,
Nguyen
Hi Nguyen,
if I use RAM based linker file (e.g. 28002x_generic_ram_lnk.cmd), all the code will be written to RAM area of the device, and that means, the code will be deleted after a power reset. Is that correct?
Correct.
Does it also mean that we only use RAM based linker file for testing because of higher speed, and for end of line product we have to use FLASH based linker file (with ramfunc attribute if needed)?
Correct.
Regards,
Vivek Singh