This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
My customer are using F28388S for development, when they generate the hex file, they find that CMBANK0_BOOTLOADER section (address from 0x00200008) in cmd file was not used, but the hex file contain the code in these address and the code is not all 0xff or 0x00, could you help explain why? for more detail please refer to these hex and cmd file attached.
Hi,
Can you share the .map file as well?
Regards,
Veena