This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: TBCLKSYNC to sync PWM9 and PWM10

Part Number: TMS320F28075

Hi,

my customer is using F28075, and they need to configure PWM1-8 72kHz, PWM9-12 60kHz.

Due to the limitation of the EPWMxSYNCI, they can't sync PWM10 to PWM9, they can only sync PWM10 to PWM7.

So they would like to try to TBCLKSYNC to sync PWM10 with PWM9.

Can we guarantee that PWM10 and PWM9 are always synced with TBCLKSYNC? Since TBCLKSYNC will only take effect one time at the beginning.

Is it possible that there will be some error(for example one or two clock mismatch) when the PWM runs for a long time?