Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH
Hello,
I test DSC on test stand. For that i need to programme IT witch test soft. For that i used the XDS100V2 programmer.
When i programme my DSC an error appears. Error : C28xx: Can't Run Target CPU: (Error -1138 .....
See below the complet error message. In this screen shot the error appears in the middle of the programmation but this problème can appears later

Why sometime the programmation succed and some time i have this error ?
This problème don't appears on each card only on some.
I had monitored the EMU0/EMU1/TCK signal to compare a succeed programmation and a fail programmation.
Below the scope capture when the programmation succeed (pink : EMU0, Yellow : EMU1, Blue : TCK)

Below the scope capture when the programmation failed

The hard configuration is the same.
The EMU0 and EMU1 doesn't move, it is normal ? I thought this signal have power to change the state of the DSC ("normal mode"/Debug mode).
Does the lenght beetween the XDS100V2 and the DSC cause this trouble ?
I need your help.
Best regard,
Romain