Part Number: TMS320F28388D
Hi,
TMS320F28388D As per TMS320F2838x TRM section 45.5.14 Figure 45-13
msgRAMConfigParams.txFIFOSize = 7U; // Tx FIFO/Queue.
Now if put index =7, and get index =2, then call
MCAN_writeMsgRam(MCAN0_BASE, MCAN_MEM_TYPE_FIFO,0U, &txMsg);
//
// Enable Transmission interrupt.
//
MCAN_txBufTransIntrEnable(MCAN0_BASE, fifoStatus.putIdx,1U);
//
// Add request for transmission.
//
MCAN_txBufAddReq(MCAN0_BASE, fifoStatus.putIdx);
after that ,I want to kown if the put index = 0 ? In other words, Is the FIFo circle FIFO?