This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: Probe supplied Power Mode but unable to debug and program using XDS110 debug probe

Part Number: TMS320F28027F

Hello 

I am using XDS110 debug probe with TMS320F28027F controller. In Target Configuration tab, I configured the Power selection to "Probe supplied Power " voltage to 3.3V. 

But following is the error occurred...

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\yash\AppData\Local\TEXASI~1\CCS\
ccs1031\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Apr 29 2021'.
The library build time was '17:49:40'.
The library package version is '9.3.0.00058'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-267' (0xfffffef5).
The title is 'SC_ERR_XDS110_TARGET_SUPPLY'.

The explanation is:
The controller could not detect valid target supply. Check target
JTAG connection and/or connection setting specifying voltage level.

[End: Texas Instruments XDS110 USB Debug Probe_0]

 

I have connected TMS, TDI, 3V3, TDO, TCK, TRSTn and GND pins 

Connector used -  CTI20(IN)-TI14(OUT) JTAG ADAPTER

Following is Screenshot of Target Configuration - 

After saving and configuring the debug probe, 0V is measured across 3V3 and GND pins