This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Using strobe event latch with ADC SOC on eQEP

Part Number: TMS320F28388D

Hi,

For a project I need to read ADC acquisitions and position encoders at precise moments.

In the design, ADC SOCs are synchronized by the PWM event triggers (TBCTR at zero) and generate an IT at the end of the conversions. eQEP must be read during the same PWM event and I generate an IT too.

In the TRM (27.5.2.2 Strobe Event Latch), it is mentioned that it is possible to latch position counter from external pin or ADCSOCA & B.

Do you have more information on the way to use this function in order to reduce the number of ITs?

Sincerely.

Jerome