Hi,
Is there a subtle difference between implementation of the McBSP on the 2812 and the 2833x? I have an application which has been working for years on a 2812 but fails when ported to a 28335. Upon close inspection of the reference guides for the two device, they are basically the same but the 2833x guide (SPRUFB7a) contains the following note that is missing from the 281x guide (SPRU061c):

This restrcition may explain the problem I am seeing - question is does this it also apply to the 2812 and is omitted from the reference guide by mistake? Or does the 2812 not have this requirement?
Cheers,
John.