Other Parts Discussed in Thread: C2000WARE
Hi,
We are using TMS320F280048CPMQR, 64 pin PQFP for one of our applications. The development was completed using XDS100V2 debug probe. When I tried to flash the code, flashing is happening but after power cycling the code is not getting executed. Following are the steps performed.
1) Change the debug configuration to "release" and selected it as "active".
2) Excluded RAM_link.cmd file from the project and added F280048C_Flash_link.cmd. (One strange thing happened. The project build failed. The compiler include options were not the same as that of the normal debug session. Added all those and build is successful).
3) Invoked debugging session.
4) Unlike normal debugging, it takes few seconds more and displaying messages like erasing memory location, do not cancel etc.
5) After that it returns without any error in the console.
6) On disconnecting the debug probe and power cycle. The total current taken is 60mA less than when normal debug execution using the probe.
7) In my code a GPIO is continuously toggled, which is not happening. The flashing was repeated 2-3 times but with same behavior.
8) If I invoke normal debug session, its working fine.
Please see anything wrong with the process or any additional steps are required, Any help or advice will be much appreciated.
Thanks and Regards
Karthik R