Part Number: TMS320F28377S
Other Parts Discussed in Thread: TIDM-1010, TMS320F28379D
Hi~
I have a question about the 28377S and BISS-C communication connection.
Referring to the document below, it is explained that BISS-C communication is connected only when CLB is built-in.
For the 28377, which doesn't have a built-in CLB, I'm curious how to connect the BISS-C communication.
If only RS485 communication is configured without CLB, is BISS-C communication possible?
Reference document. :
TIDM-1010
BiSS-C Absolute Encoder, Master-Interface Reference
Design for C2000 MCUs
| 2.3.2 | PM Biss-C Master Implementation Details This section gives a brief overview of how the BiSS-C interface is implemented on TMS320F28379D |
devices. By design the TIDM-1010 device works with multiple C2000 LaunchPad development kits. This
reference design focuses on the F28379D LaunchPad as the main example.
Communication over the BiSS-C interface is primarily achieved by the following components:
• CPU (C28x)
• Configurable logic block (CLB)
• Serial peripheral interface (SPI)
• Device interconnects (XBARs)