This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
When I use the SCI flash kernel to generate .txt file, but it report the error: fatal error: cannot open input file "–o.out": No such file or directory
Board: F28032
Demo: C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f2802x\examples\structs\f28027_flash_kernel
So is there anything I missed?
Can you right click on the project and select properties. Then click on the C2000 Hex Utility and take a screenshot of that window, specifically the summary of flags set? I think the -a is for ascii output, but I'm not sure why there are symbols past this flag. You may need to go through the C2000 Hex Utility and see if you can find where this symbol is set.
Best,
Matthew