Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE
Greetings! I am trying to build my frequency inverter program. So I want to add multiple options for the user to spin the motor as V/F, simple FB, FOC and so on. To achieve this i have to add multiple .c files as links to the project from the instaSPIN library. So when ctrl.c file is not included to my project the motorID function works perfectly. But when I add it, this cuases an overcurrent error. I just linked it to the project, i removed every code attempting to use this .c file -> no luck. Can you advice me what to do?
Thanks!