This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: EPWM output when low pulse width will not satisfy the desired Deadband

Part Number: TMS320F280049C

For a complementary EPWM1 output to drive a half-bridge IGBT/SiC module, I will be using the "activehigh complementarty dead-bead mode" with equal RED and FED.

EPWM1 is operated in the up-down count mode.

If RED/FED is greater than the original pulse width (i.e. before a deadband is implemented), what will be the actual outputs at the processor pins?

This question is arising since with my SVPWM at certain modulation indices, I could get some original pulses (i.e. before a deadband is implemented)

with pulse widths less than or equal to RED/FED.

Thanks

David