Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH
Hi TI,
I have a brand new TMS320F28335 Experimenter Kit that I just purchased. I am attempting to program and run a simple PLECs/Simulink model on the board that generates two PWM signals and reads a voltage from a potentiometer with the ADC. When I build and program the model it functions exactly as I expect, with no errors displayed. However, when if I power cycle the board it loses the program and is back to factory settings and I must build/flash the model again. This requires me to always have the board plugged into my computer in order to flash the program every time.
I've also tried to use CCS as well as just MATLAB Simulink's C2000 coder (no PLECs) to blink an LED and have the program save to flash (standalone). However after power cycling the board memory is completely wiped again.
Is there a particular setting or jumper configuration required in order for the TMS320F28335 to boot from flash and start running the saved program/model?
I've attached images of my PLECs coder configuration and Uniflash settings.
Thank you,
Tom