Hello!! champs
There is a part in my program that writes and erases data in the FLASH (0x83000) area.
If you set DCSM as follows,

An error occurs when data is written to and deleted from FLASH.

In this regard, the questions are as follows:
1. Is it impossible to read/write in the FLASH area when DCSM is set?
1-1. Is there a workaround if this is not possible?
Please answer.
We always appreciate your help.