Other Parts Discussed in Thread: C2000-GANG
Device: TMS320F280049
1. The first question is ERROR 354 appears when the TXT file is opened in C2000-GANG. As shown below:
2. And the second question is after opening the HEX file and clicking Save to image, the software crashes. But when using the HEX file compiled by another project, there was no problem when clicked Save to image. In CCS, the HEX file generation setting items are the same for these two projects, so it is suspected that it is related to the HEX file, but it is not clear where the problem is.
Add one information, the self-test of the tool is passed as below:
Could you pls help review and give some comments on these two questions? Thanks!
Best Regards,
Sherman