This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
I have a question about the BOOSTXL-POSMGR board being used with a sin/cos encoder, In the user manual, it says that they used the IDDK board along with the POS MGR is this necessary? Is there an option to use this without the IDDK? Can you confirm?
Also, I checked the user manual of the POSMGR for the SinCos encoder, However, it didn't include details on hardware connection or pins connection. Can you also provide this?
Thanks in advance.
Regards,
Marvin
Marvin,
The BOOSTXL-POSMGR + LaunchPad can be used. It will require some pinout changes in the code. The source code is in controlSUITE so this can be done by your customer.
Regards
Lori