Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello,
I am trying the test the sci flash programmer for F28379D controlCARD R1.3 and controlCard DOcking Station R4.1.
I am using C2000Ware3.4 and the precompiled executables and .txt hex files at C2000Ware/utilities/flash_programmers/serial_flash_programmer
I have connected win10 host computer via usb to uart ftdi converter cable to GPIO84/85. I have tested this serial connection using the c2000ware sci echoback example with necessary pin mux changes. I am able to echo characters back succefully using putty connected to the COM port.
I have tried to put the card into SCI boot mode via the dip switch A:SW1 on the controlCARD. it is set to 01.
In order to program I run the following command in the console and autobaud fails to lock

I've seen many other questions on this board which usually are due to a bad serial connection or wanting to use GPIO28/29 for connection. I know my serial conneciton works and I'm trying to use default pins. What could be cauing autobaud to not lock?
I have probed the pins on the experimenter kit with a signal analyzer. I could see the host send 'a' once then no other activity on either serial line.
Please advise!