Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi,
I am following the Serial Flash Programming of C2000 Microcontrollers App Note in order to get SCI programming working on my LAUNCHXL-F28P65X.
At the moment I am getting stuck at the point that the "serial_flash_programmer" running in Visual Studio reaches the "Attempting autobaud to load kernel..." as shown here:
My SCI UART Select Switch - S2 (0:1) and Boot Select Switch - S3 (0:1) are shown here:

I am trying to follow the troubleshooting question below in the app note.
7 Troubleshooting - 7.4 F28P65x - Question: With the LaunchPad, I cannot download the SCI Flash Kernel to RAM in SCI Boot, what steps should I take to do so?
But the "Answer:" does not make sense in some places. It seems to be referring to the ControlCARD and not the LAUNCHXL-F28P65X when mentioning the FTDI Chip and opening the Memory Window in CCS to change values in memory.
Can someone assist me in getting this working?
My ultimate goal is to use EtherCAT FoE to download the firmware to the C2000 and using the Live Firmware Update Without Device Reset on C2000 to perform a Live Firmware Update.
Thanks,
Rob McCullough