Other Parts Discussed in Thread: C2000WARE
Hello Champs,
Customer had SVPWM related questions for "universal_motorcontrol_lab_f28002x" project in C2000ware Motorcontrol SDK (using FAST library):
1) Is SVPWM used in this project 5-stage or 7-stage?
2) Which value of below "SVM_Mode_e" will be used in calculating current/voltage offset during offline state before starting? Which value of below "SVM_Mode_e" will be used during motor running?
//! \brief Enumeration for svpwm mode
//!
typedef enum
{
SVM_COM_C = 0, //!< SVPWM common SVM mode
SVM_MIN_C = 1, //!< DPWM minimum SVM mode
SVM_MAX_C = 2, //!< DPWM maximum SVM
SVM_DQ_S = 3 //!< SVPWM standard DQ mode
} SVM_Mode_e;
Would you please help? Thanks!
Best Regards,
Linda