Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
Hi team,
Here's re few questions from the customer may need your help:
1) The 74HC595D chip is driven with normal IO, and the manual States that the maximum clock rate is shorter than the time to execute an instruction. No delay is used in the customer's program and the drive signal output from the 74HC595 was found to be good. Clock is 60 MHz. DSP/DSC is a multi-level pipeline instruction which is faster, right? But now there's no problem. Is there anything wrong or any configuration need to be modified?
2) The program starts with MemCopy&RamfuncsLoadStart,&RamfuncsLoadEnd,&RamfuncsRunStart
Does this statement indicate that the program is executing in RAM? What should the customer do if they want code in a while loop to execute in RAM?
Could you help check this case? Thanks.
Best Regards,
Cherry