Part Number: TMS320F28069
Hi team,
Here's an issue from the customer may need your help:
Debug CAN receive stability, CAN transmit and receive normal after DSP software is running.
Then try to unplug the CAN cable and then connect the CAN device, after several consecutive plug-and-connect times, the two bit CCEs and ACKE of canes are set up, and CAN is not able to transmit or receive properly. Does ACKE relate to the hardware cable? Under what circumstances will CCE be set?
Sometimes SMA, SE errors are set, but these bits should not cause can to receive and transmit incorrectly.


Could you help check this case? Thanks.
Best Regards,
Cherry