Hi experts,
Could let us know if phase difference between ePWM5 and ePWM6 increase or not ?
When clock source of ePWM is same, that difference is fixed after ePWM sync.
"after ePWM sync" means below processor.
1) TBCTL2.bit.SYNCSELX = 1;
2) TBCTL2.bit.SYNCSELX = 0;

Because ePWM5 out a sync signal twice when EPWMxSYNCO = CMPC,
ePWM6 counter is unexpected count-up/down behavior when ePWM6 is up-down mode.

Therefore we need to output one-shot SYNCO signal with CMPC.
We have a question. After one-shot sync, a phase difference between ePWM5 and ePWM6 is fixed ?
We expect that it is fixed because a clock source of ePWM is same.

Best regards,
Hidehiko