Part Number: TMS320F280049
Hi Champ,
I have two question for eCAP/ePWM sync function as following:
1.if eCAP6 configure to use EXTSYNCIN1 as sync input, and configure GPIO0 as EXTSYNCIN1 through input XBAR.
how many SYSCLK delay from the GPIO0 rising edge to the CTRPHS be load to TSCTR? this delay clock is fixed or not fixed?
2. Based on my testing ,if eCAP6 enable HRCAP function, the EXTSYNCIN1 sync function cannot work, but if I disable the HRCAP function, the EXTSYNCIN1 sync function can work normally. May I know the reason?
3.If ePWM1 configure to use EXTSYNCIN1 as sync input, and configure GPIO10 as EXTSYNCIN1 through input XBAR.
how many SYSCLK delay from the GPIO10 raise edge to the TBPHS be load to TBCTR? this delay clock is fixed or not fixed?