Part Number: TMS320F28377D
Hello,
I am having issues connecting the JTAG to the C28377D processor after programming the DCSM (pwdlock is not yet programmed).
During testing, I programmed the DCSM password first. This would still work.
I then programmed the GRABSECT/GRABRAM in OTP

Now, the device is in low power mode when trying to connect via JTAG.

From other forums, it is indicated that I should use "WAIT BOOT" in this case.
how can I externally change the EMUBOOT data in ram, if this is now in a secured area?
The EMUBOOT was originally programmed to BOOT TO FLASH (0x0B).
how do you recommend starting "wait boot" externally?
Thanks,
Jesus