This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I read the Tformat encoder using SCI, I made the CRC calculation as follows. The code before __flip() of the bit string was difficult to understand, and I thought that __flip() would not be necessary when reading from SCI, so I made it. If I have missed something, please let me know.
#include "device.h"
#include "driverlib.h"
void SCI_tformat_generateCRCTable(uint16_t *pTable)
{
uint16_t i, j;
uint16_t accum;
uint16_t polynomial = 0x0081;
for(i = 0; i < 256 ; i++)
{
accum = i;
for( j = 0; j < 8; j++)
{
if(accum & 0x0001)
{
accum = ((accum >> 1) & 0xFF) ^ polynomial;
}
else
{
accum = ((accum >> 1) & 0xFF);
}
}
pTable[i] = accum;
}
}
uint16_t SCI_tformat_getCRC( uint16_t * msg, uint16_t *crcTable, uint16_t rxLen)
{
uint16_t i;
uint16_t accum = 0;
int *pdata;
pdata = (int *)msg;
for (i = 0; i < rxLen; i++) {
accum = crcTable[(accum ^ __byte(pdata,i)) & 0xFF] ^ (accum >> 8);
}
return accum;
}
Hi,
Can you please provide details on the issue you are facing? Also, were you using any reference code from TI?
Regards,
Veena
In PM_tformat_getCRC of PM_tformat_crc.c file, there is the following statement, which I do not understand why it is necessary. I would like to know if the specific 2 bytes need to be processed differently even for data from SCI where the bit sequence is not inverted this time.
//
// Do the first two bytes, special case
//
i = crcAccum ^ (__byte(pdata, index--));
crcAccum = crcTable[i] ^ crcAccumLow;
i = crcAccum ^ (__byte(pdata, index--));
crcAccum = crcTable[i];
Translated with www.DeepL.com/Translator (free version)
Hi,
I will check with the module owner and get back to you
Regards,
Veena
Hello - is the code provided not working ? I don't recall the specifics of the implementation - however it was tested with an actual encoder responding to the commands.
Thank you or your replay.
This is the CRC when SCI is used for Tformat instead of SPI, since SCI does not invert the bit sequence like as SPI does.
I don't understand why the first 2 bytes are special case when using SPI. Is this the case with SCI also a special case?
The CRC routine provided is very generic and will work with different lengths of data. Since the T-Format data is always a multiple of 8, it can be simplified. I'm not sure the bit of code you mention is even used for T-Format. My suggestion is to step through the code with SPI data to get a feel for what data it is using and what code is being executed and which is skipped. Then apply the same to your own application.
Hello, thank you for your reply.
Since the current hardware is connected to SCI, I created this code exclusively for SCI to read the CRC.
What I want to know is that I don't understand why your SPI code treats the first 2 bytes specially. I am not asking if my code works or not. I just don't understand why the first two bytes are a special case.
Please tell me why the first two bytes are a special case.
Unfortunately I don't recall the specifics - this code was written a long time ago. From the code, it seems to only a special case if crcAccum is set to something different in the previous if-then code. For T-format, I believe crcAccum will always be 0xFF since the number of bits is always a multiple of 8. I would have to step through the code to see if I am correct. There are a lot of CRC algorithms and code examples out on the web.
Thank you for your answer.
For a long time I did not understand how this special case could happen. This time, it is 8 bits and there is no bit inversion, so I think that the special case will not occur.
If the calculation does not match, there must be some kind of bug, or if not, it must be a hardware problem.