Part Number: TMS320F280049C
Hi Champs,
I ask this for our customer.
1. Since LS RAM can be encrypted, CLA-to-CPU can not. Is this understanding correct?
The encrypted area can access CPU-to-CLA RAM, that is, the encrypted CLA area can get the data transmitted from the CPU
But the CPU cannot obtain the encrypted data in the CLA through CLA-to-CPU RAM

2. Customer now have a problem that when they are not using DCSM, the code runs fine, but after using DCSM, when the code is run without decryption, the encrypted CLA fails to access the data of CPU-TO-CLA (data by DAC output, output is 0).
I checked the configuration of the customer's .cmd file and there should be no errors that unencrypted RAM to access encrypted RAM. Couls you help analyze the reason? Thanks!
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to Flash" bootloader mode */
/* not boot used*/
BEGIN : origin = 0x080000, length = 0x000002
CLA_PROG_RAM : origin = 0x008000, length = 0x003800
RESET : origin = 0x3FFFC0, length = 0x000002
RAMGS1 : origin = 0x00E000, length = 0x002000
RAMGS2 : origin = 0x010000, length = 0x002000
/* Flash sectors */
/* BANK 0 */
HEADERINFO : origin = 0x084000, length = 0x000100, fill 0xFFFF /* on-chip Flash */
CPU_PROG_FLASH : origin = 0x084102, length = 0x00BEFE/* on-chip Flash */
/* BANK 1 */
CLA_PROG_FLASH : origin = 0x090000, length = 0x004000 /* on-chip Flash */
FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000 /* on-chip Flash */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000F3 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMLS7 : origin = 0x00B800, length = 0x0007F8
RAM_STACK : origin = 0x00C000, length = 0x000C00
RAMGS0 : origin = 0x00CC00, length = 0x001400
RAMGS3 : origin = 0x012000, length = 0x002000
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0, ALIGN(4)
.text : >>CPU_PROG_FLASH, PAGE = 0, ALIGN(4)
.cinit : > CPU_PROG_FLASH, PAGE = 0, ALIGN(4)
.pinit : > CPU_PROG_FLASH, PAGE = 0, ALIGN(4)
.switch : > CPU_PROG_FLASH, PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.cio : > RAMGS1, PAGE = 0
.stack : > RAM_STACK, PAGE = 1
.ebss : > RAMGS0, PAGE = 1
.esysmem : > RAMGS3, PAGE = 1
.econst : > CPU_PROG_FLASH, PAGE = 0, ALIGN(4)
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS3, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
/* CLA specific sections */
Cla1Prog : LOAD = CLA_PROG_FLASH,
RUN = CLA_PROG_RAM,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
/*.TI.ramfunc : LOAD = CPU_PROG_FLASH, */
GROUP
{
.TI.ramfunc
{ -l F021_API_F28004x_FPU32.lib}
} LOAD = CPU_PROG_FLASH,
RUN = RAMGS1 | RAMGS2,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
.scratchpad : > RAMLS7, PAGE = 1
.bss_cla : > RAMLS7, PAGE = 1
Cla1DataRam : > RAMLS7, PAGE = 1
.const_cla : LOAD = CLA_PROG_FLASH,
RUN = CLA_PROG_RAM,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
PAGE = 0
CodeInfoFile : > HEADERINFO, PAGE = 0
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Best Regards,
Julia