This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28379D: How to run code in standalone on TMDSCNCD28379D control card R1.3 & Docking station

Part Number: TMDSCNCD28379D

Hello TI Team,

I am using TMDSCNCD28379D control card R1.3 with controlCard docking station R4.1. Using this board I want to run the code standalone with external +5V Input power connector J1 without need of connecting JTAG connector to my Laptop and run in debug mode in CCS.

I have tried the all the combinations with A:SW1 and SW1 but I am unable to do so. Could you please help me out what switch or jumper combinations do I have to select ? Also are there any settings I need to do in my code to run it in standalone mode ?

Thanks,

Vishal Dongare