Part Number: TMS320F28388D
Other Parts Discussed in Thread: UNIFLASH
We are currently trying to implement the Serial Flash Programmer functionality in production. However, we are having difficulty uploading the production version of the firmware to the processor.
When we include the functionality to set the DCSM Password in the output HEX file. We get either a checksum error or a blank error (If the processor was preprogrammed). Here is the file we are including (in addition to the password file itself), We can't seem to find anything specific to cause the problems. If we compile to an .OUT file and use UniFlash to send it to the processor everything works properly.
/* this linker command file is to be included if user wants to use the DCSM feature on the device
* DCSM means Dual Zone Code Security Module.
* This linker command file works as an addendum ot the already existing Flash/RAM linker command file
* that the project has.
* The sections in the *_ZoneSelectBlock.asm source file is linked as per the commands given in the file
* NOTE - please note fill=0xFFFF, this helps if users include this file in the project by mistake and
* doesn't provide the needed proper *_ZoneSelectBlock.asm sources .
* Please refer to the Blinky DCSM example in the controlsuite examples for proper usage of this.
*
* Once users are confident that they want to program the passwords in OTP, the DSECT section type can be removed.
*
*/
MEMORY
{
PAGE 0 : /* Program Memory */
/* Z1 OTP. LinkPointers */
DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00000C
/* Z1 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x000004
/* Z1 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z1_CRCLOCK : origin = 0x78014, length = 0x000004
/* Z1 OTP. RESERVED/BOOTCTRL */
DCSM_OTP_Z1_BOOTCTRL : origin = 0x7801C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z1 OTP. Z1 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000010
DCSM_ZSEL_Z1_P1 : origin = 0x78030, length = 0x000010
DCSM_ZSEL_Z1_P2 : origin = 0x78040, length = 0x000010
DCSM_ZSEL_Z1_P3 : origin = 0x78050, length = 0x000010
DCSM_ZSEL_Z1_P4 : origin = 0x78060, length = 0x000010
DCSM_ZSEL_Z1_P5 : origin = 0x78070, length = 0x000010
DCSM_ZSEL_Z1_P6 : origin = 0x78080, length = 0x000010
DCSM_ZSEL_Z1_P7 : origin = 0x78090, length = 0x000010
DCSM_ZSEL_Z1_P8 : origin = 0x780A0, length = 0x000010
DCSM_ZSEL_Z1_P9 : origin = 0x780B0, length = 0x000010
DCSM_ZSEL_Z1_P10 : origin = 0x780C0, length = 0x000010
/* Z2 OTP. LinkPointers */
DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00000C
/* Z2 OTP. GPREG1/GPREG2 */
DCSM_OTP_Z2_GPREG : origin = 0x7820C, length = 0x000004
/* Z2 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x000004
/* Z2 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z2_CRCLOCK : origin = 0x78214, length = 0x000004
/* Z2 OTP. GPREG3/BOOTCTRL */
DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z2 OTP. Z2 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000010
}
SECTIONS
{
dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0//, type = DSECT
dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0//, type = DSECT
dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0//, type = DSECT
dcsm_otp_z1_bootctrl : > DCSM_OTP_Z1_BOOTCTRL PAGE = 0//, type = DSECT
dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0//, type = DSECT
// dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P1 PAGE = 0//, type = DSECT
dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0, type = DSECT
dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_bootctrl : > DCSM_OTP_Z2_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0, type = DSECT
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Are there any ideas as to what could be causing the problem. We've been able to overcome everything else so far including the (Align 8) issue.
Ben