Part Number: TMS320F280049C
Hello,
I am using a custom board with F280049C for developmental purposes with code running in RAM.
Debugger: Xds110 in 2 wire mode.
Now, as the code size increases, I get linker errors which indicate that all SARAM space has been utilized.
To resolve this issue would it be possible to:
1. RUN new code which is to be tested, from RAM.
2. The older code , which has been tested, remains in FLASH and can be accessed.
This would avoid frequent FLASH programming and also reduce the time to test.
regards.