Hello,
I have an annoying problem because my bootloader works very well most of the time. However, I have some hardware that when used misses the first bit from the master. All of the hardware is the same, just different cards.
My bootloader is set up with a SPI slave config, below is the SPI config code and my RX and TX interrupts:
void SPI_Init() { Interrupt_register(INT_SPIA_RX, &spiaRxFIFOISR); Interrupt_register(INT_SPIA_TX, &spiaTxFIFOISR);//TX //SPIA_slave initialization SPI_disableModule(REPA_DSPI_SLAVE_BASEADDR); SPI_setConfig(REPA_DSPI_SLAVE_BASEADDR, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0, SPI_MODE_SLAVE, 500000, 8); SPI_enableFIFO(REPA_DSPI_SLAVE_BASEADDR); SPI_setFIFOInterruptLevel(REPA_DSPI_SLAVE_BASEADDR, SPI_FIFO_TXEMPTY, SPI_FIFO_RX8); SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_TXFF);//TX SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF); SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF_OVERFLOW); SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RX_OVERRUN); SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RX_DATA_TX_EMPTY); SPI_enableInterrupt(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF); SPI_enableInterrupt(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_TXFF);//TX SPI_disableLoopback(REPA_DSPI_SLAVE_BASEADDR); SPI_setEmulationMode(REPA_DSPI_SLAVE_BASEADDR, SPI_EMULATION_FREE_RUN); SPI_enableModule(REPA_DSPI_SLAVE_BASEADDR); Interrupt_enable(INT_SPIA_TX);//TX Interrupt_enable(INT_SPIA_RX); } __interrupt void spiaTxFIFOISR(void) { uint16_t i,SendingByte; for(i = 0; i < 8; i++) { //SPI_writeDataNonBlocking(REPA_DSPI_SLAVE_BASEADDR, sBuffer[sbufferindex]); if(NumnberOfDatatoSend>0){ if(sbufferindex ==90){ SendingByte = sBuffer[90]<<9 | ((sBuffer[0] & 0x80)<<1); sBuffer[90] = 0; sbufferindex = 0; }else{ SendingByte = sBuffer[sbufferindex]<<9 | ((sBuffer[sbufferindex+1] & 0x80)<<1); sBuffer[sbufferindex]=0; sbufferindex++; } //SendingByte = sBuffer[sbufferindex++]<<8; //if(sbufferindex==90)sbufferindex =0; SPI_writeDataNonBlocking(REPA_DSPI_SLAVE_BASEADDR, SendingByte); NumnberOfDatatoSend--; } else SPI_writeDataNonBlocking(REPA_DSPI_SLAVE_BASEADDR, 0); } // printf("running"); SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_TXFF); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP6); } __interrupt void spiaRxFIFOISR(void) { uint16_t i,reByte; uint16_t SendingByte; // if(dataRecieved){ // SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF); // Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP6); // } for(i = 0; i < 8; i++) // while(SPI_getTxFIFOStatus(REPA_DSPI_SLAVE_BASEADDR) != SPI_FIFO_RXEMPTY) { reByte = SPI_readDataNonBlocking(REPA_DSPI_SLAVE_BASEADDR) & 0xFF; if (/*!dataRecieved && */(bufferindex !=0 || ((reByte & 0xFF) == 0x5A))) buffer[(bufferindex++ % 300)] =reByte ; } datalen = buffer[2] & 0xff; //datalen |= (buffer[3] <<8) & 0xff00; PacketsRecv = datalen + 6; if(datalen == 0 && (buffer[1] == 0xA6 || buffer[1] == 0xA1 || buffer[1] == 0xA2)) { datalen=2; PacketsRecv=2; dataRecieved=true; // SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF); }else if(bufferindex > 5 && bufferindex >= PacketsRecv){ dataRecieved=true; //SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF); } SPI_clearInterruptStatus(REPA_DSPI_SLAVE_BASEADDR, SPI_INT_RXFF); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP6); }
My master is sending 0x5A 0xA6 to ping the bootloader, the bootloader is seeing consistently 0x5A 0x26 on the hardware that does not work with the bootloader. This means I am missing bit 7 of the 2nd byte. What is interesting, is that if I change the protocol parameter in SPI_setConfig() to SPI_PROT_POL0PHA1 (Mode 1. Polarity 0, phase 1. Rising edge with delay.) or SPI_PROT_POL1PHA0(Mode 2. Polarity 1, phase 0. Falling edge without delay.) from SPI_PROT_POL0PHA0 (Mode 0. Polarity 0, phase 0. Rising edge without delay.) this fixes the read issue when using this hardware. However, the TX to the master then does not work.
What would you recommend checking here? I have the bootloader working well on 4 systems but I have 1 system and 1 card where the bootloader is missing bits. However, if I download the SPI application firmware to the board via XDS110 then the SPI works fine and does not miss bits.
Thanks for the help!