Part Number: TMS320F28379D
The sample project works with the CPU1_RAM build configuration. It does not work with the CPU1_FLASH configuration. This is with no modification to the project other than changing the active build configuration. From a bit of a look, I see that the CLA interrupt occurs only one time. I have not looked into it further.
1. This is in part to alert TI that one of its sample projects does not work as expected.
2. Is this a known issue, or do you know what the issue may be? (I was having problems with a custom project using CLA, which works from RAM, but not from Flash, which is why I started looking at this sample project. If I get the sample project working from Flash, it may help me figure out what is happening on my custom project)
Thanks!