This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
For my next project I need to know the real MIPS when application is running with 200Mhz clock from internal flash both for CPU & CLA,
as per www.ti.com/lit/an/spra958l/spra958l.pdf (dated 2013, 5 years ago) with @150Mhz clock uC can achive 90 - 95 MIPS
Now i need the same updated values for 200Mhz clock with the new TMS320F28379D flash tecnology.
Fa,
Thanks for reaching out to the forum. There are 2 key differences between the Flash architectures in the F2837x devices vs the ones in the Application Report you have referenced:
1)0 Wait State access time
2)Prefech Buffer Depth
Just to keep things simple I'm going to use the F2833x as the baseline "previous gen" device for comparison. All of the below are documented in the respective DS, except for the approx speed; since this is based on some assumptions of 16-bit/32-bit code use and typical control code continuities
Device | Max CPU Speed | 0 WS Max Flash Speed | WS at max CPU speed | Pretech buffer depth | Approx Flash speed |
F2833x | 150MHz | 27MHz | 5 | 64-bits | ~90-95 MIPs |
F2837x | 200MHz | 50MHz | 3 | 128-bits | ~174-188 MIPs |
Best,
Matthew