Other Parts Discussed in Thread: C2000WARE
Team,
Can you please help with the below question?
For our project we would like to support variable frequency mode where rising and falling edge for PWM signal are determined based on two external events.
My idea was shown in Figure which I attached, where triggers T1 and T2 for Action qualifier are used:
What I don´t know and what is not clear is if we select for example DCAEVT1 to be source for T1
-then can we use blanking period?
It is not clear if blanking is used just for the signals which comes to the trip-zone. It is not clear from where DCAEVT1 comes.
-Does it come before filtering module or it can go also through the filtering module?
Here blanking would be very important for us, so that we can limit the minimum Off-time.
If we cannot use blanking with T1 and T2 than I suppose the only option is to use Cycle-By-Cycle Trip event.
-Blanking should be included while using CBC. correct?
-Can Triggers T1 and T2 be blanked if connected to Digital Compare submodule?
Or is blanking only possible is trip is used?
-Any existing code examples you can refer to?
Thanks in advance,
A.