Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi,
as already asked and solved in other questions I'm trying to use the CLA math library with F2838xCPU1_CLADATAROM_Symbols_fpu32.lib in a TMS320F28388 project with --vcu_support=vcrc option turned on.
But I receive the same linker error: <F2838x_CPU1_ROM_out_CLALnTable_tmp.obj>" has a Tag_VCU attribute value of "1" that is different than one previously seen ("3"); combining incompatible files
I'm using libs from C2000Ware 4.03 and CGT 22.6.
Links to other similar questions:
As stated by an answer in the last link there should be an updated version somewhere in C2000. But I can't find it...
Please help.
Thanks,
Daniel