This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm developing a firmware for the device TMS320F280025.
My current CCS version is "12.2.0.00009 ".
I've faced a strange behavior.
I'm using the CCS example "flashapi_ex1_programming" and it can be correctly compiled.
The issue is related to the output generated.
If I change the output format in ""BUILD / C2000 Hex Utility / Output Format Option" I get the following result:
Here below the general settings in "BUILD / C2000 Hex Utility / General Options".
The firmware generated are in the zip attached.
I noticed that the HEX and SREC fw compiled are missing one byte yes and one byte no.
You can check it by opening the file, but I try to show it better here below:
The same happens with the SREC file.
It looks like the file are cropped.
Is there a reason for this bug?
Is there an option in the compiler to get the HEX/SREC file with the same data as BIN file?
Regards,
The likely fix is to add the option --romwidth=16. To understand why, please see this forum post. Though ignore the parts about the length of the line. That is not a concern here.
Thanks and regards,
-George
Hi George,
Is this a workaround to use "-romwidth=16" or an intentional thing that at default it should be preset?
Otherwise I add that line as you can see:
The two files are different at the bottom:
Actually this is not a big deal because I can continue with my work, this was just my curiosity.
Best regards
Is this a workaround to use "-romwidth=16"
No. The default is inherited from the predecessor toolchain for C28x, which started in the mid 1980s. At that time, a default of --romwidth=8 made sense. It does not make sense today. But we have learned, over the years, that changing a long standing default creates more problems than it solves.
Thanks and regards,
-George