Part Number: TMS320F280039C
Hi,
I am using a SCI in address mode and I try to detect a BRKDT character sent by a different device (Slave). The BRKDT in SCIRXST does not set to be set even if I short the RX line to ground times to times. Simulate BRK.
What are exact condition for the break character bit to be set. According to spec, it has to be at least 9.625 bits. Is there a maximum? My other device is sending 13 bits at 0. (I am using 8 bits data + address mode (no parity).
- What is the difference compare to frame error (FE bits)? Is it also set even if data is 0?
- If I get a BRKDT detected, is RXRDY bit set also with the corresponding RX buffer (SCIRXBUF) at 0?
Thanks,
Arnaud